10/7/2020 5:31 AM | |
Posts: 1 Rating: (0) |
Can you please prepare a sample program of poke block in tia v15.1 and how to check in which db data is sent If we are using 0 for receiving db. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/07/2020 10:46:58New subject after splitting |
|
10/7/2020 11:12 AM | |
Joined: 3/30/2020 Last visit: 9/19/2024 Posts: 4767 Rating: (978) |
Hello. Have a look at the sample library provided by Siemens: This has far more than what you ask for so it will be helpful for your future enquiries also. See the picture to guide you on where to find the relevant sample. Note the PEEK / POKE commands are SCL instructions. Mr. Denilson Pegaia packaged this in a FB that can be used in LAD code. The DB number is zero if that number is not of importance; it is only used when referencing from a DB. Read/Write from/to inputs / outputs / memory-bits does not use the DB number. The in-software help is very descriptive about those instructions. I would encourage you to have a look at the help provided there. You may even find that you do not need an extended example. PRO TIP: (terms and conditions apply) BR |
Last edited by: qwazee at: 10/07/2020 11:18:04Last edited by: qwazee at: 10/07/2020 11:18:43Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on