10/1/2020 10:06 AM | |
Posts: 22 Rating: (0) |
Dear experts I have an S5-100U PLC CPU 103 Ref: 6ES5 103-8MA02 The orange battery LED is on (as shown in the attached photo), I would like to know if there is a battery change procedure and what is the reference of the battery that I can find on the market to change it. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/01/2020 12:31:05New subject after splitting |
|
10/1/2020 12:28 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello Amine; The procedure for battery replacement on a S5-100U is very similar than for a S5-95U above, simply make the battery exchange while the PLC is powered-up; see section 4.4.2 of the manual: https://support.industry.siemens.com/cs/ww/en/view/1091978 Here is one possible link to purchasing a replacement battery for a S5-100U, more are available using Google: https://www.amazon.com/Replacement-SIEMENS-SIMATIC-S5-100U-Battery/dp/B07MTZ8CPQ Hope this helps, |
Last edited by: dchartier at: 10/01/2020 12:34:46 |
|
10/7/2020 3:16 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello Amine; As long as your provider is proposing Tadiran batteries as replacements for a S5-100U, you should ask him for a SL-350, considered by Siemens as an adequate replacement part for a S5-100U battery, Siemens part number: 6ES5 980 0MA11 https://support.industry.siemens.com/cs/ww/en/view/7379933 S5-100U replacement battery: Li battery, size 1/2 AA, 3.6V/ 0.85Ah 6ES5 980 0MA11 --->Tadiran SL-350 Technical data sheets for the Tadiran SL-350: https://support.industry.siemens.com/cs/ww/en/view/68057757 The screenshot below is taken from the Tadiran battery catalog: https://tadiranbatteries.de/pdf/product-data-catalogue-tadiran-lithium-batteries.pdf Hope this helps, |
Follow us on