10/8/2020 7:36 AM | |
Posts: 2 Rating: (0) |
Dear Siemens Experts, I have the same issue, I have restored the %TE and %TO files to the system, There are also there are R-Parameters, which I have entered them manually. I noticed there are Background Buffer Parameters, which I could not change them manually, what should I do, why is the green start key keep flashing, where I could not jog or reference the axis (no alarm shown on the screen)? I attach here a video showing the problem, and a photo showing the BACKGROUND-BUFFER data which I try to input but it shows Entry Disabled (while the input key is enabled). Please help.me. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/08/2020 10:13:10New subject after splitting |
|
10/8/2020 8:28 PM | |
Posts: 2 Rating: (0) |
I can't move axis. There is no error message, but green "not in position" LED lights up together with red LED above (see attachment). |
Follow us on