10/9/2020 11:04 AM | |
Joined: 4/28/2015 Last visit: 4/24/2024 Posts: 320 Rating: (35) |
Hi, By collision "monitoring" are you referring to Collision Avoidance? The older release notes for Sinutrain V4.5 SP2 mention in the foot notes: "The new SINUMERIK feature "SINUMERIK Collision Avoidance" is NOT released for SinuTrain for SINUMERIK Operate V4.5." However in the later V4.5 Edition 3 release (based on actual software V4.5 SP6 HF3) Collision avoidance is listed as an option in the template machines (screenshot attached) and no such foot note entry exists in the release notes. I hope this helps Luke.N |
This contribution was helpful to1 thankful Users |
Follow us on