10/10/2020 10:33 PM | |
Posts: 3 Rating: (0) |
Ok, I will write in English |
10/10/2020 11:01 PM | |
Posts: 3 Rating: (0) |
Hi, I want to know if you could help me. I have a program, which I have previously proof in the testbench and it worked. But by the time I tried to load it in the machine, the machine doesn't work at 100%. I would like to know if you could help me, the only outs that work are Q1 and Q8 and the rest of the program doesn't run properly. Perhaps the problems is related to the nesting depth of the programe, I'm not sure. The machine is a thermoforming one. I send you the file of my programe in order to ask you if you could help me, please. Thank you very much. AttachmentTermoformadora_30-09-2020_0BA8_no funciona.zip (100 Downloads) |
Follow us on