10/12/2020 12:07 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, Unit_PLC is mandatory to occupy units when a Batch is activated. Also it handles communication with the Batch Server. The other blocks you describe are you used if you want to manually configure Equipment Operations, Equipment Phases, or parameters (Tag_Coll). Mainly you will use those blocks if you do not use a SFC type/instance or want to use additional conditions for example: Start the next unit allocation if a level is reached. The level can be connected to a Tag_Coll block which is basically a collection of parameters enabled to use in Batch Configuration. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on