10/12/2020 8:19 AM | |
Posts: 4 Rating: (0) |
Dear Technology Team, Thank you for the reply. I am also having the same problem of fixing the set value. As you mentioned ( and also in manual) P2253 is Tec_ctrl_setp1, which is having scaling in PERCENT.
But the problem is when I try to set set 50% of the Analog input is my set point, In drive the parameter already settled to P2224 which is a read only parameter.( image attached below) Here I was little bit baffled, not able to go forward for setup of my setpoint. Thanks in advance for the help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2020 13:20:23New subject after splitting |
|
10/12/2020 1:22 PM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7953 Rating: (162) |
Closed cause question posted twice. The second thread with the subject G120x Multi pump control SETPOINT problem is published within the conference SINAMICS. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on