10/6/2020 10:12 AM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054)
|
Hi wmr1986 "Instance DB, word access, Access address: 2104" means that FB 7922 is trying to access DBW 2104 in its Instance DB. The "Module Address" name is bit misleading and is simply a reference to place inside FB 7922 where the access to the Instance DBW 2104 occurs. As Umencho suggested, use the "Go To" button for the Event log entry and it will take you right to place where the problem occurred. |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on