10/12/2020 8:09 PM | |
Joined: 9/3/2008 Last visit: 5/8/2024 Posts: 921 Rating: (158) |
Hi FredMau If you have copied and pasted your code directly into the post, then the issue is that you have a space in the if ... then statement so that the variable "Value5" has become "Value 5" (see below):
If this is not the reason, then I suggest you debug by inserting the following lines just before the if ... then statement:
Then you can see the output in the diagnostic window and perhaps see what is happening. |
Michael |
|
This contribution was helpful to1 thankful Users |
Follow us on