10/14/2020 9:54 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927)
|
Hi, The manual is very unclear about this, but these parameters have something to do with Plant Automation Accelerator. In PAA, you can interconnect blocks like functions. There references are created and likewise stored in these variables you mention. I tried to use them in PCS7 only, but it's not working. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
10/15/2020 5:51 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927)
|
Yes, correct , I know but did you test this with a type and instance the project? Because that is not working , the instantiation process |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on