10/16/2020 10:59 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi again, Interesting questions When the object is deleted from CMT, it will be deleted from the CM (instance). If you delete the object from the CM, but not from CMT, during the next synchronization, the object is added again to the CM. But since update of Update Collection 2 for PCS7 V9.0 SP2 (I believe...not 100% sure), the CM instances cannot be changed anymore like changing default values or interconnections between objects inside the CM instance. You have to work from the CMT or you have to set "Ignore" property (indicated by a pink color) to enable change of that value inside the CM. See the following link for synchronization behaviour: Synchronization of CMT |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on