10/14/2020 8:50 PM | |||||||||
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello,
Perhaps the following points might help: CPU 1214C, DC/DC/DC, 14DI/10DO/2AI
2-Perform the method as in the attached file. What is the Version of The TIA Portal Project? 4- To upload the TIA project ,you should use the same TIA Portal version that used previously to download the project into the CPU. |
||||||||
Eng.Mohamed Ibrahim |
|||||||||
10/16/2020 2:19 AM | |
Posts: 7 Rating: (0) |
Thanks to all. Just to be sure that I have correctly understood: regarding what is explained here https://support.industry.siemens.com/cs/ww/en/view/97554052 Option N: I create a new project, without device configuration, and after marked the project name I follow the instruction Option S: I create a new project with an identical device configuration as I can check on site, and after marked the PLC station I follow the instruction Is that correct? In order to perform it, I imagine is better to put the PLC in stop. Or it is not necessary? |
Last edited by: Jen_Moderator at: 10/16/2020 10:35:21Optimized link. |
|
10/17/2020 8:05 PM | |
Posts: 7 Rating: (0) |
Thanks a lot to all. I will try, hoping to be lucky! |
Follow us on