10/19/2020 10:31 AM | |
Joined: 9/26/2018 Last visit: 9/19/2024 Posts: 2 Rating: (0) |
Could you please propose a Siemens's loadcell model that is suitable for this application? Thank you very much. |
10/19/2020 1:38 PM | |
Joined: 1/4/2007 Last visit: 9/2/2024 Posts: 1142 Rating: (175)
|
Hello Ronald20101990, in your first post, you wrote, that the load cell has a capacity of 20 kg. Therefore, I recommend you to use this load cell: WL260 SP-S AA (Aluminium), 20 kg: 7MH5102-2GD00 See also the attached file, please. This load cell is for a platform max. 400mm x 400mm. But you will measure your object in the middle of the platform. Best regards Siwarexi
AttachmentWL260 SP-S AA.pdf (283 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on