10/13/2020 5:37 AM | |
Joined: 12/27/2019 Last visit: 7/26/2024 Posts: 1 Rating: (0) |
Hello, I have same problem but for my case my HMI can export log to sd card without problem at first, but after one month this error suddenly keep pop up. Only for one log but other log can export without problem. ( Error 80045) Is it possible that my sd card have problem because when i check my sd card it is very hot. I did try format my sd card and restart HMI, then the problem gone. But after few days, the error keep pop up again. Is there a way to correct to error? I am using Kingston 16GB Sd card Thanks for any help Amar ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/13/2020 12:15:09New subject after splitting |
|
10/21/2020 3:50 PM | |
Joined: 8/3/2009 Last visit: 9/24/2024 Posts: 13778 Rating: (1741)
|
Hello drive542 The Error description tells that the Storage is not available or Full. It is also not a good idea to use such a big SD Card in a Comfort Panel. The released Siemens SD Card for the Panels are 2GB. Here some information: https://support.industry.siemens.com/cs/ww/en/view/95853895 The System alarm tells also that a Timeout is reached and that the System tries to do the Export later again. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on