10/22/2020 5:58 PM | |
Joined: 1/17/2013 Last visit: 4/11/2024 Posts: 1079 Rating: (6) |
Dear Expert. As picture my network consist of 1.PLC Third part 2.CU320-2DP 3.PLC AB SLC5/05 LAN 4.PLC S7-1215C 5.MAIN HMI TP1500 Comfort 6.Slave HMI TP900 Comfort How the easy way TP900 comfort can control and monitor PLC as TP1500 ? Best Regards, Vorapob AttachmentTP1500 TP900 PLC Network.pptx (191 Downloads) |
Best Regards, |
|
10/23/2020 7:11 AM | |
Joined: 1/17/2013 Last visit: 4/11/2024 Posts: 1079 Rating: (6) |
Dear Madadi , I would like use 2 panel as the same time same function in both panel same screen. How can I do please ? Best Regards., Vorapob |
Best Regards, |
|
10/23/2020 9:42 AM | |
Joined: 1/17/2013 Last visit: 4/11/2024 Posts: 1079 Rating: (6) |
DearMadadi, I would like to use 2 Panel TP1500 and TP900 have same function and operator can control machine in both panel but TP900 have only 1 IP address while TP1500 have 2 IP address. How can TP900 can connect all PLC and 1 CU320.-2DP as TP1500 ? Best Regards, Vorapob |
Best Regards, |
|
10/23/2020 7:45 PM | |
Joined: 12/28/2016 Last visit: 4/19/2024 Posts: 427 Rating: (44) |
I suggest two ways to do this. 1-Get all TP1500 tags via s7 1200 (cpu 1215) In this case, TP900 can receive these tags via s71200. 2-Connect between TP1500 and TP900. To do this, please read the following page 👇 HMI to HMI communication |
https://pnap.ir |
|
Follow us on