10/24/2020 3:21 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066) |
Perhaps this? SIMATIC HMI KTP400 Basic Panel, Key/touch operation, 4" TFT display, 65536 colors, PROFINET interface Order number: 6AV2123-2DB03-0AX0 A TIA V11 can't open with TIA V16 directly. First you have to upgrade the TIA V11 project to TIA V13 SP1 (or SP2). Then the upgraded V13 project can be upgraded to TIA V16.
|
This contribution was helpful to1 thankful Users |
10/25/2020 2:43 PM | |
Joined: 11/16/2019 Last visit: 2/12/2024 Posts: 32 Rating: (0) |
Ok. Then I need v11, v13, and v15? |
10/25/2020 5:35 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066) |
No. You need V13 SP1 (or SP2) and V16. Why do you ask for V15? |
Follow us on