10/27/2020 7:37 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, User can connect analog input via PP module X3 connector. 4 channel AI can be connected, i.e. 4 wire or 3 wire type. 2 PT100 analog inputs & 2 nos 0.. 10 V analog inputs can be connected either in mA or voltage type. You need to convert your external analog signal either in 4.. 20 mA or 0..10 Volt & then connect it to PP module. Also needs to modify PLC hardware project, define AI, write a logic & download it in PLC. Please refer SINUMERIK 828D PPU and components manual chapter 7.8.3.4 for more detail information. HTH |
Last edited by: Jen_Moderator at: 10/27/2020 09:58:46Optimized link. |
|
Follow us on