5/24/2017 5:54 PM | |
Joined: 4/21/2015 Last visit: 4/19/2022 Posts: 18 Rating: (0) |
Same issue with me i am using siemens 1500 with dp connected to 2 no of identical g120 cu 240e- 2 dp v4.7 . My all commands are going through hardwire only the current refference i am taking through profibus .. now one vfd is having no issue but one vfd is continoussly tripping in F01910. i try to increase the monitoring time also but it didnt work . I disable the fault using p2100 and p2101 but still i am getting this fault .. now one more thing while getting this error cpu is healthy, even though the vfd is not showing any bus fault ., it is just tripping and the ready led is turning into red any suggestions?? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/26/2017 8:17:30 AMNew subject after splitting |
|
5/29/2017 5:08 PM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Hello AutoGen_1041985, 1. Check the wiring (interrupts of the cable) Make a trace of the r 2050.0 and r2050.1 triggered onto fault. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
10/27/2020 8:57 PM |
|
Joined: 9/2/2015 Last visit: 3/21/2022 Posts: 1 Rating: (0) |
...sent from App |
Follow us on