10/29/2020 9:07 AM | |
Joined: 4/24/2006 Last visit: 9/18/2024 Posts: 8738 Rating: (1168) |
Hello, When you have 6ES7214-1HG40-0XB0, you need at least TIA Portal v13, see this link: Sales/Delivery Release: S7-1200 CPU V4.0, CPU 1217C and IO-Link Master SM 1278 Perhaps this link might help: Best regards, Wizard |
This contribution was helpful to1 thankful Users |
10/29/2020 9:13 AM | |
Joined: 5/9/2019 Last visit: 9/10/2024 Posts: 53 Rating: (2) |
Did you try this? |
Best regards, John. |
|
10/29/2020 9:22 AM | |
Joined: 7/21/2009 Last visit: 9/9/2024 Posts: 12 Rating: (1) |
I tried this in Tia v12. It loaded the hw config. but the software upload was not still possible. In Tia v13 I think I tried this options with sample project also. I didn't try to use the unspecified PLC with v13 because there was the PLC in Tia's HW catalog. But in Tia v13 I got the error that the project is in v12.0 and I have v13.0. Edit: Is it possible to copy the program to Flash Card and than upload the program from Flash Card to PC?
I had the V13.0 Tia.
I looked at the second link. They propose to use the unspecified 1500 CPU to upload the program. Is it OK I tried to use the unspecified 1200 CPU since I have the 1214 PLC? Edit2: Is it perhaps possible to download some HSP package to update the HW catalog of PLCs in Tia v12? I tried to download the package for Tia v12 (packages) but there are not any new PLCs. Is there maybe some other source I can use to get the 6ES7214-1HG40-0XB0 plc into the v12 Tia? |
Last edited by: krala at: 10/29/2020 09:23:33Last edited by: krala at: 10/29/2020 09:24:07Last edited by: krala at: 10/29/2020 09:25:33Last edited by: krala at: 10/29/2020 09:26:19Last edited by: krala at: 10/29/2020 09:52:54Last edited by: krala at: 10/29/2020 09:53:41Last edited by: krala at: 10/29/2020 09:54:02Last edited by: krala at: 10/29/2020 09:58:55Last edited by: krala at: 10/29/2020 09:59:56Last edited by: krala at: 10/29/2020 10:00:26Last edited by: krala at: 10/29/2020 10:01:12Last edited by: krala at: 10/29/2020 10:01:51 |
|
Follow us on