Industry Online Support
Technical Forum
10/29/2020 9:35 PM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32992 Rating: (4076)
|
I can only assume that you mean the error when the LOGO! has switched to STOP at irregular intervals during network communication. This happened with the LOGO! 0BA8.Standard with firmware version FS03. LOGO! 0BA8.Standard with FS01 or FS02 did not have this error. As the 0BA8.Standard does not yet have the firmware update function, the error could not be repaired. Only the FS4-LOGO!s no longer had this error and the firmware can also be updated.
AttachmentVersions of 0BA8.txt (206 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on