10/30/2020 1:22 PM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
OK, but Siemens put it there for a reason... which is that, then? |
10/30/2020 1:52 PM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
OK, thank you for clearing that out. |
10/31/2020 5:55 AM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32990 Rating: (4076)
|
This only makes sense if (depending on the LOGO! Series) the program on the card is write-protected. Since LOGO! 8.1 with FS05, parameter changes are saved on an existing SD card during runtime. Sales and Delivery Release for LOGO! 8 BM FS05 and LOGO! Soft Comfort V8.1.1 (SP1) |
This contribution was helpful to1 thankful Users |
Follow us on