9/17/2017 9:53 PM | |
Joined: 12/20/2016 Last visit: 4/19/2024 Posts: 11 Rating: (0) |
Greetings, Does anyone know how the GSD for Danfoss FC280 can be installed on Step 7 V5.3? Or how the GSD file can be modified so it can be installed? (GSD attached) If I use Step 7 V5.4 or later the GSD install is correct and no error is shown, so the easy solution is to update to V5.4.. However I have to use V5.3 LOG: GSD installation ---------------- Beginning: 9/17/2017 12:59:12 PM Source directory: C:\Documents and Settings\Administrador\Escritorio\PB GSD files_FC280 Target computer: PCS7 User: Administrador File: DANF040F.gsd Status: Not installed. Error while verifying GSD file. S7HWCNFX.EXE: Install GSD File (13:4951): Errors in DANF040F.GSD, line 218: the textual descriptions, which reference the 'ExtUserPrmData' definition, contain at least one parameter value not valid for this parameter. S7HWCNFX.EXE: Install GSD File (13:4951): Errors in DANF040F.GSD, line 223: the textual descriptions, which reference the 'ExtUserPrmData' definition, contain at least one parameter value not valid for this parameter. S7HWCNFX.EXE: Install GSD File (13:4951): Errors in DANF040F.GSD, line 268: the textual descriptions, which reference the 'ExtUserPrmData' definition, contain at least one parameter value not valid for this parameter. S7HWCNFX.EXE: Install GSD File (13:4951): Errors in DANF040F.GSD, line 273: the textual descriptions, which reference the 'ExtUserPrmData' definition, contain at least one parameter value not valid for this parameter. S7HWCNFX.EXE: Install GSD File (13:4663): 4 errors were found in the GSD file (type file) DANF040F.GSD. S7HWCNFX.EXE: Install GSD File (13:4341): The GSD file (type file) C:\DOCUMENTS AND SETTINGS\ADMINISTRADOR\ESCRITORIO\PB GSD FILES_FC280\DANF040F.GSD contains syntax errors. The DP slave that is being written to by this file therefore cannot be transferred to the Hardware Catalog. ----------------------------------------------------------------------------------------------------- AttachmentPB GSD files_FC280.zip (691 Downloads) |
11/2/2020 5:59 AM | |
Joined: 11/12/2019 Last visit: 5/30/2022 Posts: 1 Rating: (0) |
what pass and username |
11/2/2020 6:55 AM | |
Joined: 5/12/2006 Last visit: 4/24/2024 Posts: 22226 Rating: (2980) |
what you mean? |
10/22/2021 2:07 PM | |
Joined: 4/16/2021 Last visit: 11/12/2023 Posts: 1 Rating: (0) |
Hello, I perform a gsd file for the FC280 Danfoss drive. But, the plc (S7- 300) didn't recognize the drive (via step7 5.6 in HW config.) and show the warning 34. The new drive is use to substitute the VLT2800 which is out of service. The FC280 gsd was downloaded from Danfoss site. It seems like the problem is the gsd file. need help please ! AttachmentVLT_FC280_PROFIBUS_GSD_2016-10-10.zip (347 Downloads) |
10/25/2021 12:32 PM | |
Joined: 2/11/2015 Last visit: 4/24/2024 Posts: 437 Rating: (33) |
Pay attention at the PROFIBUS Type, if it's DPV0 or DPV1
AttachmentVLT_PROFIBUS_GSD_2010-11-03.zip (350 Downloads) |
Follow us on