10/2/2020 1:19 AM | |
Joined: 12/12/2013 Last visit: 9/11/2024 Posts: 31 Rating: (1) |
I have found myself at this same junction. I have opened a screen using the script below, and would like to close it also after a time. --------------------------------------------------------Start Script #include "apdefap.h" int gscAction( void ) { #define PIC_0 "ParticularPopupScreen.pdl" SSMOpenTopField('1',PIC_0);//Return-Type: BOOL return 0; } --------------------------------------------------------End Script From reading above is sounds like this may not be the best way to achieve this, is there a better way/command to open a popup that makes it much more straight forward to close? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/02/2020 07:37:23New subject after splitting |
|
Follow us on