11/9/2020 1:33 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. I need to add a new WinCC button to make it possible for the operators to make a time limited override of a condition. I can find the buttons (1-106) in the Tag manager and I can see where they are used in the picture (not used after Button_101) . Most of the buttons (but not all) are controlled be the block WinCCButton (FC1129) so I can find all these by doing a cross-reference on this block but is there really not a better way to see where they all are used (perhaps even the ones that are not with FC1129)? AttachmentButtons.zip (57 Downloads) |
Follow us on