11/9/2020 2:07 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, It is referring to a project inside your multiproject. I get these warning sometimes as well. If you press on button: Details, you can see which object is causing this. It could be the OS server project or a client project. I suggest you open the OS project (server of client, to where it is referring to) and close it via Close project. Then try again. Sometimes it helps to restart Simatic Manager or a reboot. If that doesn't fix the issue, you can do the following: 1. Close all open project except the one you want to archive 2. Open SQL Configuration Manager via the Start button 3. Go to SQL Server Services and right click on: SQL Server (WinCC) and press: "Stop" 4. Archive the project and after it has finished, go to SQL Server (WinCC) and press: "Start" |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on