11/1/2020 8:45 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear EBM101, Let me organize a bit. Assuming you have 1 AS (AS01), 1 x OS Server (OSS), 1 x OS Server Standby (OSS_Stby). 1. What is your original project setup in your simatic manager? is it a multiproject with 2 x user projects (1 AS and 1 OS Project) (Setup Type A)? or 1 x user project with AS and OSS inside the project (Setup Type B)? 2. Why are you adding another user project? 3. If you are using setup type A, have you done the merging of Plant bus network in the "Adjust Multiproject setting" at the top of the multiproject (in component view)? 4. In the netpro settings, is the name of the s7 connections for OSS to AS01 and OSS_Stby to AS01 the same? for example, if the name is "OSS_AS01" in OSS station wincc appl, it must be identical in OSS_Stby wincc appl as well. This is to share the same connection and tags. 5. when compile OS , are you selecting "Named Connection" in the compilation dialog? Hope these questions help you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on