11/14/2020 3:54 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Fikrr; The screenshot you show us shows a valid Profibus-DP configuration for your scale. It also shows that the data (IN and OUT) is taken as a single consistent telegram, "4W consistent" for both lines in your I/O table. This will require that you use SFC 14 "DPRD_DAT" and SFC 15 "DPWR_DAT" in your PCS 7 program See the entries for these functions in the System and Standard Functions manual: https://support.industry.siemens.com/cs/ww/en/view/109751826 These SFCs were developed for use with Simatic Manager and Step 7 v5.x.For information on their use with PCS 7, look at these pages from the PCS 7 V9.0 SP1 Manual Collection https://support.industry.siemens.com/cs/ww/en/view/109759321/113683549835 CPU 41x–H as PROFIBUS DP master https://support.industry.siemens.com/cs/ww/en/view/109759321/31144120715 Consistent Reading and Writing of Data from and to DP Standard Slaves/IO Devices https://support.industry.siemens.com/cs/ww/en/view/109759321/113683549835 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/14/2020 16:03:56 |
|
This contribution was helpful to1 thankful Users |
11/15/2020 3:23 PM | |
Joined: 2/12/2019 Last visit: 7/30/2024 Posts: 17 Rating: (0) |
Hello dchartier Thank you for supporting me I am new in PCS7 & Profibus DP and facing some problem, may it is very basic I insert new DB1 to store data from Scale, but download button is disable. I have followed instruction in this forum to change PCS7 become Step7 in object properties ->general -> use then result is "unable to copy..." Please find the attachment Thank you Fikrr Attachmentdownload disable.zip (62 Downloads) |
Follow us on