11/17/2020 12:14 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. I need to show a number (it will be an integer) on one of my HMI pics. The number is stored in DB8.DBW28. I have added this value (now it is named DB8,DD28) to my WinCC tags under the right PLC and given it the name Caterp_2_Counter_Value. But when I look at the display the number is shown as 0 even though it is 14 in the PLC. Why is it showing the value as 0 and how do I get it to show the correct value? AttachmentFD2 Smøresekvens A.zip (49 Downloads) |
11/17/2020 1:39 PM | |
Joined: 6/19/2019 Last visit: 4/26/2024 Posts: 690 Rating: (72) |
Hello, Maybe change in HMI data type becose now it's float type. |
This contribution was helpful to1 thankful Users |
11/17/2020 3:09 PM | |
Joined: 1/15/2018 Last visit: 4/29/2024 Posts: 145 Rating: (5) |
Hi, A DBW is an integer. A real is DBD. Best regards, Gonzalo |
This contribution was helpful to1 thankful Users |
Follow us on