11/18/2020 6:09 PM | |
Joined: 7/7/2010 Last visit: 4/17/2024 Posts: 14593 Rating: (2346) |
https://flows.nodered.org/node/node-red-contrib-s7 may help, but you may need to have a PLC connected to the CU320 to use Node Red. Here's the generic S7 Node search results: https://flows.nodered.org/search?term=s7 If you know about Profinet, S7, and Sinamics drives, you may be able to use an existing Node Red S7 communications, you may be able to make it work similar to how people got it to work for Logo8 devices ( https://flows.nodered.org/flow/f36b5e6ef46f3a2c3d9c26eb45cbad0d ). If you have a PLC controlling a CU320 / servo drive / motor, you first need to change the telegram to also send motor temperature (assuming the motor has an internal temperature sensor). If you do not have a PLC connected, it might be a lot less expensive / difficult to add a TC to the motor paired with a separate NodeRed capable TC signal conditioner.
|
Last edited by: 0_Einstein at: 11/18/2020 18:15:43science guy |
|
Follow us on