11/29/2020 10:10 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Are you sure about S210 drives? Is any specific reason? Max motor power & torque available with S210 drive & 1FK2 motor is 7KW & 40 Nm for 3 phase AC 400 V supply. Is this ok? If yes, please refer SINUMERIK MC mit S210 als NC Achse (OEM), SINUMERIK MC MCU commissioning: NC, PLC, Drive Commissioning Manual & 109769849-Application_SINUMERIK_MC_with_SINAMICS_S210_as_NC_axis_en.pdf . documents. HTH |
Last edited by: Jen_Moderator at: 11/30/2020 11:04:10Optimized links. |
|
11/29/2020 12:28 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please refer Application example for the configuration of the technology objects combined with SINAMICS S210 which may help you. |
11/29/2020 2:53 PM | |
Joined: 1/17/2013 Last visit: 9/18/2024 Posts: 1103 Rating: (6) |
Dear PISCEAN 2010, I never use SINUMERIK PLC before. My application use max. torque 10 Nm 3 max power 8 KW. phase AC 400 V supply. Can you suggest me How to use torque control and 2 axis synchronize as well ? Thank you. Best Regards, Vorapob |
Best Regards, |
|
12/2/2020 6:00 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, I do not have exact project as per your requirement. However here with please refer below links which shall be help you to understand set up of Sinumerik CNC system, PLC hardware etc. etc. SINUMERIK 840D sl: STEP7 Toolbox for SINUMERIK - Programming recommendation for changers Winder function with tension control (OEM / distributor) SINUMERIK 840D sl: STEP 7 project be archived as „SINUMERIK (*.ARC)“ Bellow function manual will help you (TRAILON) function shall be best applicable to your requirement, but I do not have any project or sample PLC logic of the same. SINUMERIK 840D sl / 828D special functions Yes with Sinumerik 840D SL + S120 you can configure 4 Nm servo motor also. All the best. |
Last edited by: Jen_Moderator at: 12/02/2020 07:24:02Optimized links. |
|
12/2/2020 4:45 PM | |
Joined: 1/17/2013 Last visit: 9/18/2024 Posts: 1103 Rating: (6) |
Dear PISCEAN 2010, How to open program from this web as picture ? What is the software use to open this program ? Best Regards, Vorapob AttachmentHow to open Program.jpg.zip (428 Downloads) |
Best Regards, |
|
12/3/2020 4:38 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Couldnot view files since error is displayed. Please refer attached snap. |
Follow us on