12/1/2020 6:30 AM | |
Joined: 6/19/2017 Last visit: 4/19/2024 Posts: 7961 Rating: (162) |
Hi FRANCK HERVE, Please try to discuss your question in English language. This is an international community and we try to focus on one language. Posting in English will help you to get more response to your question. This is the translation of your question:
Best regards, |
My Forum is the place to personalize your profile, |
|
12/2/2020 3:48 PM | |
Joined: 2/10/2015 Last visit: 4/10/2024 Posts: 285 Rating: (1) |
Is it possible to download a project edited under SIMOTION SCOUT with STARTER from a SINAMICS inverter. |
12/2/2020 4:09 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979)
|
download (to inverter) or Upload (from inverter) ? |
12/2/2020 4:13 PM | |
Joined: 2/10/2015 Last visit: 4/10/2024 Posts: 285 Rating: (1) |
in both directions, i.e. upload from and download to |
12/2/2020 4:21 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979)
|
upload from yes download to yes if you first perform upload from |
12/2/2020 6:33 PM | |
Joined: 2/10/2015 Last visit: 4/10/2024 Posts: 285 Rating: (1) |
In access point, I chose S7ONLINE and in PG / PC parameter, I chose my ethernet network card But, when I start the search for subscribers, I see the first message (add IP address / subnet masks) and I clicked on yes. Some time later, I perceive the second message telling me no device was found. I have STARTER V5.4.0.1 HF1 that I have installed and I don't know if the version of SINAMICS D425, CU320, S120 they used may not exist in my version of STARTER. When I installed SIMOTION SCOUT I managed to open the SIMOTION SCOUT source project from the simatic manager and I went online without problem. But, I uninstalled simotion to install starter because there is a machine with sinamic inverters programmed with starter. as I cannot have simotion and starter on my pc at the same time then, I decided to have starter alone and work with on the different machines. since i uninstalled simotion when i open my main project with simatic manager i have this software missing error message yet i have starter on the pc. see attached file.
AttachmentFILES.zip (172 Downloads) |
Follow us on