12/3/2020 1:10 PM | |
Joined: 10/25/2018 Last visit: 4/4/2024 Posts: 4 Rating: (0) |
Sir, We are using simoreg dc drive model no-6RA7081-6DV62-O-Z , In this drive we done the auto tuning , the motor is running smoothly but the field voltage increases as rpm increases The field voltage is starting from 220 vdc and goes upto 350 vdc, due to this the motor field winding heat up and motor fail also. So suggest any field parameter to make the field voltage constant.Your support is very much helpful. Thanking You , Ranjit Kumar ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/04/2020 06:54:55New subject after splitting |
|
12/4/2020 6:57 AM | |
Joined: 6/19/2017 Last visit: 4/18/2024 Posts: 7933 Rating: (162) |
Closed cause question posted twice. The second thread with the subject Simoreg DC drive 6RA7081-6DV62-0-Z field voltage and current not control is published within the conference DC converters SIMOREG. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on