12/2/2020 12:44 AM | |
Posts: 4 Rating: (0) |
I have the same G120 CU240E-2PN , I set up all this settings, I want to start with 80% of torque, but I do not know what else should I do after? P96: [Expert] P1300: [22] Torque Control (encoderless) Macro: [5] Conveyor Technology with Fieldbus and Basic Safety Telegram: [352] Siemens telegram 352, PZD-6/6 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/02/2020 11:00:49New subject after splitting |
|
12/2/2020 8:19 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Which is PLC? Have you connected drive with PLC? Have you established connection & communication between PLC & drive? Have you open project & configured hardware in project? Have you download project in PLC & drive? Which software you use for drive? Findout answers to above points. Understand earlier posts by experts which will help you to set up communication & parameterization of drive. Please refer below links for more detail information. SINAMICS G120 CU230P-2; CU240B-2; CU240E-2 Control Units Installation and parametrization of a SINAMICS G120 (Videos) SINAMICS G/S: Speed control of a G120/S120 with S7-300/400 (STEP 7 V5) via PROFINET (PROFINET RT) SINAMICS G120 converter with Control Units CU230P-2; CU240B-2; CU240E-2 |
Last edited by: PISCEAN 2010 at: 12/02/2020 08:21:08Last edited by: Jen_Moderator at: 12/02/2020 11:02:56Optimized link. |
|
Follow us on