12/3/2020 8:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, 6SL3210-5BB13-7UV1 is not compatible with 6SL3210-5BB13-7AV0. Successor drive for 6SL3210-5BB13-7AV0 is 6SL3210-5BB13-7BV1. |
12/3/2020 9:09 AM | |
Joined: 5/9/2019 Last visit: 9/10/2024 Posts: 53 Rating: (2) |
Hello, thanks for your answer. I saw that it was not the succesor that siemens advises, but I though it was compatible, maybe it had some different measure or no fan compared to the previous one. So if it has the same parameters is it impossible to make the replacement although its controlled via DI? Thanks for your answer. |
Best regards, John. |
|
12/3/2020 9:14 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
with DI, control should be possible. |
12/3/2020 9:46 AM | |
Joined: 5/9/2019 Last visit: 9/10/2024 Posts: 53 Rating: (2) |
I though it could be some electrical problem related to the configuration, but if it was that i suppouse the drive would notify it, they just power off 2 seconds after i reset the emergency on the cell, and it falls over again. Is necessary an autotune? I programmed it only connected to power line, no other wires connected to it. |
Best regards, John. |
|
Follow us on