12/8/2020 2:22 AM | |
Joined: 8/17/2020 Last visit: 1/8/2023 Posts: 27 Rating: (1) |
Hello- I am still new to LOGO! although I have build a few projects. This is my first attempt at analog and I am having a problem I have the input and scaling from a 4-20 ma pressure transducer working correctly. In fact, with the built in simulator everything works. When I download the program to LOGO! I received an error. It seems that my min/max block output is not connected. I can't figure out what to connect the output of the min/max block to. I am trying to enable a text block so I can read the max pressure on my TDE as I would like to see the max pressure that a hydraulic circuit build to. LOGO! 6ED1052-2MD08-0BA0 TDE LCS 8.2.1 Thanks in advance AttachmentBaler Pressure Logger I.zip (133 Downloads) |
12/8/2020 4:47 AM | |
Joined: 8/17/2020 Last visit: 1/8/2023 Posts: 27 Rating: (1) |
Thank You I understand now. |
12/8/2020 4:49 AM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
But have some other problems in your program. What is the physical range of the sensor? 0 to 6.25 bar? |
Follow us on