1/29/2009 6:33 PM | |
Posts: 1 Rating: (0) |
I'm experiencing an issue with Programing an ET200M Slave on an SS52 Master using the ComProfibus v5.1.2.3 Tools. If I use the original ET 200M (IM153-1) mask file SI801DVE.200 and create the Bin file and dowload to the SS52 the drop works fine. If I use the newer SIEM801D.GSE v1.25 I get a buss fault. I've configuredboth drops identicaly. The only difference betweenn the .200 and .GSE is the addtional i/o cards that are available and that I am looking at using in my application. When I inspected the .bin files I notice the new file has addtional code that it downloads to the SS52, mainly the slave descriptors. Attachmentdata.zip (378 Downloads) |
Follow us on