12/24/2020 12:36 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, You would need to use Server Data editor. At the client project on the ES in WinCC Explorer you can go to Server Data and right click and select "Configure". Under column: "Preferred Server" you can select the master or standby server for each server package. Do this for each client and download the clients. PS: Server Data must be already generated for the client |
Last edited by: Oreca at: 12/24/2020 12:40:23Last edited by: Oreca at: 12/25/2020 10:15:37Made the post more clear If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
12/25/2020 10:13 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, Yes, always work on the client project on the ES and download to the client. If you work on the client directly, you may loose changes when somebody else downloads the client from the ES. PS: It was not very clear in my previous post. I will change it |
Last edited by: Oreca at: 12/25/2020 10:14:12If I could help you, you can use the RATE button. Thank you. |
|
Follow us on