1/4/2021 12:16 PM | |
Joined: 12/31/2020 Last visit: 6/24/2022 Posts: 3 Rating: (0) |
I have a SIEMENS LOGO PLC! 8 6ed1052-1cc08-0ba0 24CE programmed to store in the SD memory the data connected to an analog input. I want to know if it is possible to access the SD through the LOGO ACCESS TOOL and see the historical data in Excel program. I've installed the complement "LOGO! access tool" in Excel, but when I try to access into the PLC by IP address the Excel program reports "error 91 at run time". I am using MS Office professional plus 2010. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 01/04/2021 13:25:02New subject after splitting |
|
1/4/2021 1:26 PM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
closed cause question posted twice. The second thread with the subject Is it possible to access the SD through the LOGO ACCESS TOOL is published within the same conference LOGO! - Software Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on