1/5/2021 10:34 AM | |
Joined: 2/24/2020 Last visit: 5/18/2022 Posts: 7 Rating: (0) |
Sorry, my mistake here is the file
AttachmentOil Protection.zip (140 Downloads) |
1/5/2021 10:50 AM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
I added two more threshold triggers. These have "0-20mA" as a sensor type. 0 mA corresponds to 0 units, 4 mA corresponds to 200 units. The output of the threshold trigger switches on at 0,0 mA and off at 3.8 mA. You only have to specify where you connect the outputs of the threshold triggers.
AttachmentLub Oil_V2.zip (143 Downloads) |
This contribution was helpful to1 thankful Users |
1/5/2021 11:14 AM | |
Joined: 2/24/2020 Last visit: 5/18/2022 Posts: 7 Rating: (0) |
Amazing!! Thanks a Lot! |
This contribution was helpful to1 thankful Users |
1/5/2021 2:55 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
|
Follow us on