1/9/2021 5:10 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
What is mean by ES client and Master ES? Means you set up engineering station as a OS Client? to troubleshoot the performance , turn on task manager -> performance to check CPU loading and RAM usage. You can check resource monitor to have detail look on CPU usage. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/10/2021 11:02 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
For multiuser engineering , i prefer the method of "remove from editing / remove from multiproject" You may use this method if you have station granular setup, where your AS projects are separated with your OS projects. For your case, im not sure on the reason. Is it a permanent situation or only because of specific stations? |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/10/2021 7:28 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927)
|
Hi, Well, Siemens hands out a few tips when using multi user/multi project engineering. One specifically is about the chart compilation and download. It is recommended to do this on the ES server (main ES) or use remote access to the main ES and execute compilation/download. Using PC's with high clock rates, lots of memory, SSD disks is recommended. Also the connection between PC stations should be a gigabit network (recommended). Also archiving multiprojects is not recommended to do via the network. One other point is the OS compilation which should be done always from only from one PC station, like the ES main server. All with all, I guess the best thing to do is editing charts via ES client and when compilation of charts is needed, to do so from the main ES (either a remote connection to the main ES or physically on the main ES. Other users cannot work on the project during AS compilation so that should not be an issue.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to3 thankful Users |
Follow us on