1/12/2021 11:53 AM | |
Joined: 8/1/2012 Last visit: 7/30/2023 Posts: 178 Rating: (15) |
Dear Experts, I have faulty compile, do you have a clue for that? all the F related software is installed. check the attached to see that. here is the error text. Log: Module driver Filter: <No filter> Responsible user: Administrator Generate module driver for AS-PROJEKT\ESD-01\CR02_A03\ESD-01\ of 1/12/2021 1:42:29 PM. W: FDO10xDC24V/2A (6ES7 326-2BF10-0AB0) is not supported. W: FDI24xDC24V (6ES7 326-1BK02-0AB0) is not supported. W: FDO10xDC24V/2A (6ES7 326-2BF10-0AB0) is not supported. W: FDI24xDC24V (6ES7 326-1BK02-0AB0) is not supported. W: FDO10xDC24V/2A (6ES7 326-2BF10-0AB0) is not supported. W: FDO10xDC24V/2A (6ES7 326-2BF10-0AB0) is not supported. W: FDO10xDC24V/2A (6ES7 326-2BF10-0AB0) is not supported. W: FAI6x15Bit HART (6ES7 336-4GE00-0AB0) is not supported. W: FAI6x15Bit HART (6ES7 336-4GE00-0AB0) is not supported. W: FAI6x15Bit HART (6ES7 336-4GE00-0AB0) is not supported. W: FAI6x15Bit HART (6ES7 336-4GE00-0AB0) is not supported. W: FAI6x15Bit HART (6ES7 336-4GE00-0AB0) is not supported. E: Necessary files are missing for block F_CH_AI. Please note that you have to install exactly the same version of the library as the one this block was imported from.. >>>Due to the previous error(s), creation of module drivers was aborted<<< Many thanks in advance Mojtaba Attachmentinstalled simatic software.zip (69 Downloads) |
|
|
1/12/2021 12:53 PM | |
Posts: 198 Rating: (60) |
Hello Mojtaba, I presume the issue you are facing with compilation is due to the missing 'SIMATIC S7 F Device Integration pack' . S7 F Device Integration Pack V6.2 Upd1 as a separate download for users of F Systems V6.1 or higher. You can download it from the link below: https://support.industry.siemens.com/cs/document/109782016/simatic-s7-f-device-integration-pack Hope this helps! |
This contribution was helpful to2 thankful Users |
1/12/2021 2:15 PM | |
Joined: 8/1/2012 Last visit: 7/30/2023 Posts: 178 Rating: (15) |
thank you so much my friend.it solved by your hint. I wish you the best |
|
|
This contribution was helpful to1 thankful Users |
Follow us on