1/12/2021 6:14 PM | |
Joined: 7/2/2015 Last visit: 4/25/2024 Posts: 96 Rating: (23) |
Dear fabioga66, this FAQ could be interesting for you Which licenses exist for the WinCC/WebNavigator? - From WinCC version 6.2 on, the archive licenses are version-independent and
countable - Up to version WinCC V7.3, the WinCC options and associated licenses are downward compatible. - From WinCC version 7.3 on the following licenses are version-independent and countable: +WinCC WebUX - From WinCC version 7.4 on, the following licenses are version-independent, countable, and no longer backwards-compatible with WinCC <=V7.3: +WinCC WebNavigator +WinCC DataMonitor |
If this Information really helps, you could use the Rate function |
|
Follow us on