2/9/2019 5:57 AM | |
Joined: 7/8/2018 Last visit: 4/29/2024 Posts: 20 Rating: (0) |
Hi mike, Can LOD relay setting file in digsi 4 can be transferred to another relay having LOR communication protocol . D= MODBUS , R= IEC61850 I tried three different methods but it is not working. 1. Changing the Device MLFB using object properties and then opening the project offline & saving it. I intialize the device but it gives error write at the end could not update the parameter set. 2. I updated the parameter set i.e is LOD relay has pset= 4.62 & LOR pset = 4.77 i updated it but then also gives same error could not update prameter set. 3. Then i tried creating DEX file instead of variant file . Then also gives the same error could not update pset. Is it possible to transfer LOD relay file to LOR relay . If it is possible then what is the procedure. If it is not possible then why? Please give reply ASAP Regards Abhishek ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/11/2019 11:14:57 AMNew subject after splitting |
|
2/11/2019 9:38 AM | |
Joined: 10/9/2007 Last visit: 9/18/2024 Posts: 1249 Rating: (115)
|
hi dont Change mlfb, just Change the module type |
Energy Automation products: Sicam, Siprotec, Digsi |
|
1/14/2021 12:50 PM | |
Joined: 7/8/2018 Last visit: 4/29/2024 Posts: 20 Rating: (0) |
What is the meaning of module type please clarify |
Follow us on