1/5/2021 6:05 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, You will need Simatic Manager Step7 v 5.4 or higher (please check your NCU & system software version to confirm compatability) along with MPI CP module. I suggest you, step 7 v 5.6 with latest CP5711 (compatible with USB/MPI). Please refer STEP7_V5_6_SP1_README.pdf for detail information. Step 7 V 5.6 is also available for 21 days free trial. check STEP 7 V5.6 SP1 / STEP 7 Professional 2017 SR1 Trial Download for more information. HTH |
This contribution was helpful to1 thankful Users |
1/6/2021 11:52 PM | |
Posts: 10 Rating: (0) |
In Ohio, USA. |
1/16/2021 3:22 PM | |
Posts: 10 Rating: (0) |
I have the step 7 program downloaded from PLC. Drive x and y are not being enabled. Looks like pulse is not enabled on drive. Can someone fluent with step 7 tell what inputs & condition need to be met to enable X & Y? File attached. AttachmentS7_Fadal.zip (143 Downloads) |
1/18/2021 3:02 AM | |
Posts: 10 Rating: (0) |
No errors I think I have 5.6. There are a bunch of blocks. Never used step seven and I’m not sure how to navigate it. |
Follow us on