10/19/2010 6:35 AM | |
Joined: 10/12/2010 Last visit: 3/2/2024 Posts: 37 Rating: (0) |
HI thanks for reply me,when the plc run these faults are appear(before starting the machine) |
10/19/2010 9:34 AM | |
Joined: 6/7/2010 Last visit: 2/3/2023 Posts: 569 Rating: (37) |
Ok kambiz, after pressing the reset Sk , the alarm is appering or not ? |
Regards, |
|
10/19/2010 12:05 PM | |
Joined: 10/12/2010 Last visit: 3/2/2024 Posts: 37 Rating: (0) |
HI yes,after pressing reset sk , these faults are appear. |
1/21/2021 6:42 PM | |
Joined: 2/10/2012 Last visit: 11/14/2023 Posts: 11 Rating: (1) |
Hello. I've got the same alarms but the code that i have is 00002000H. How do you can solve those alarms? Thankyou! |
Follow us on