1/22/2021 10:25 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33799 Rating: (4199)
|
No. LOGO can only works with positive 0-10V signals. |
1/22/2021 10:29 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33799 Rating: (4199)
|
What you could do: Use an isolating amplifier that has a ± 5V input and 0-10V in output.
|
1/22/2021 10:46 AM | |
Joined: 12/13/2019 Last visit: 8/16/2022 Posts: 21 Rating: (0) |
Can you recommend one? |
1/26/2021 10:46 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33799 Rating: (4199)
|
See attachment. The programm converts 0 - 4V to -4000 - 4000rpm. AttachmentVoltage_convert_to_speed_0BA8.Standard.zip (343 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on