1/18/2021 7:27 AM | |
Joined: 1/13/2021 Last visit: 9/7/2021 Posts: 4 Rating: (1) |
Thank you very much for your answer, I will try today and I will let you know soon. |
1/23/2021 4:02 AM | |
Joined: 10/17/2007 Last visit: 9/17/2024 Posts: 4031 Rating: (353)
|
from your picture I see you did NOT make NCU clean, Please learn by yourself, --1st to clean the PLC , read page 5-40 to 5-43, (you have 840D no need to read 810D CCU) You must make LED display to "6" and only +5V green LED and PR Green LED on. or no one can help you if you can not make one time try to continue doing until you successful What do you mean by "Win XP", I said post picture your PC booting finish, and find out where you think the parameter back up to help your recovery. If you cannot make NCU working, I cannot help you remotelly You can ship your NCU to me together with NCU box and your said PC related back up inside. I will try to recover it for you PS: you PM me, you can send more pictures, but you only attached one, and Not so useful. Your picture showing NCU LED's is good
AttachmentIBN_2006.pdf (454 Downloads) |
Last edited by: nulizhang at: 01/23/2021 04:04:42If you like my comments please |
|
9/17/2021 4:38 PM | |
Posts: 1 Rating: (0) |
Hello I have the same problem in my machine. Did you solve the problem? Br RM |
5/1/2023 6:34 PM | |
Joined: 10/3/2011 Last visit: 4/12/2024 Posts: 1 Rating: (0) |
Dear, you have a wrong connection in the picture. |
Follow us on