7/21/2016 3:20 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello you don't need "mplay32.exe" and it isn't supported in Windows 7. As the FAQ you linked states, you need to use "wmplayer.exe".
Here is the TIA Version of the FAQ:
About calling the horn: I guess I would add the script to the "Incoming" Event in the properties of the Alarm. You can kill the horn by adding another script to the Events on the acknowledge tag or similar. About the big amount of alarms: If you select all 400 alarms and then add the script it's added to all of them at once. |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on