1/20/2021 3:21 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (4199)
|
Common sense should tell you that Siemens doesn't check your personal data just for the fun of it because of the software's export restrictions. And you're bypassing this review. Siemens owns the copyright to the software. If Siemens makes this software available free of charge, but requires personal data to be checked, then so be it. You do not have the copyright to the software and are therefore not allowed to circumvent Siemens' specifications and simply make this software available for download. That this whole process is annoying and time-consuming is annoying, but it is also. In any case, you do not have the right to distribute this software for free. If you don't believe me, you can write to the moderator. Here something to read for you: Why do you have to log in and register for downloading export-restricted software and what data do you need for this? |
1/20/2021 6:12 AM | |
Joined: 2/9/2016 Last visit: 8/19/2024 Posts: 56 Rating: (4) |
Ok, I understand you, but I don't like you putting me in a position like distributing illegal software here in offiial forum.I was just trying to help.The user only waits for the support emploeyee to click on the registration application, which is not subject to any special conditions or even conditional on payment.The user bought Siemens HW and got into a situation that he is not able to start the project just because Siemens has unhappily set up the distribution in 8.3.I have published only a mirror of the official link: https://support.industry.siemens.com/cs/ww/en/view/109783154 Okay, next time I won't get involved ... |
Last edited by: Jen_Moderator at: 01/20/2021 07:09:04Optimized link. |
|
1/20/2021 9:22 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
Hello Mara2000, thank you that you tried to help. I'm glad, that there are so many members, which are willing to be for assistance. I have to agree with ixo65. If somebody need a software that is restricted according national and European export regulations and US re-export regulations he or she has to wait until the check is done. Alternatives:
The restriction has no relationship whether you have bought the software or not. The update contains part that shouldn't be delivered in every country of the world. Here information that are available via Wikipedia regarding Export Administration Regulations Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on