1/25/2021 5:42 PM | |
Posts: 12 Rating: (0) |
how |
1/25/2021 8:35 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417) |
Ok, I did some more of your work for you. Sinamics G120 CU240E-2PN P2000 - Entries - Forum - Industry Support - Siemens (https://support.industry.siemens.com/tf//WW/en/posts/sinamics-g120-cu240e-2pn-p2000/193024 )
In your case, a 50 Hz motor rated @ 1470 rpm needs 340Hz output. If your drive is configured for Dynamic Drive Control, the maximum rpm you can achieve is ~7050 rpm. Is that what you are reaching? |
Last edited by: 0_Einstein at: 01/29/2021 20:03:33math correction: 7050 rpm science guy |
|
This contribution was helpful to1 thankful Users |
1/29/2021 6:54 PM | |
Posts: 12 Rating: (0) |
i m reaching maximum rpm 7200 dynamics control, if i go cu 250s how much rpm can i achive |
Follow us on